VLT® High-Power frequency converters are the new medicine in China
24 September 2009
An analysis of operations at Chinese pharmaceuticals company, Harbin Lanxing Group, revealed potential for energy saving – up to 30 percent - in its process equipment on a raw medicine product line.
The company therefore decided to have two high-voltage motors including oxidation fans and a glycol motor upgraded by using two high-power VLT® AutomationDrives.
The Harbin Lanxing Group is so satisfied with the result that it now wants to upgrade the company’s remaining six high-voltage motors with direct start-up.